|
Directives 94/9/EC and ATEX95 specify new regulations for explosion protection for all types of devices for the European market.
These directives also apply to industrial gear units of the MC series and planetary gear units. As of July 1, 2003, directive
94/9/EC applies without limitations to the use of industrial gear units of the MC and X series and planetary gearmotors within
the European Union. Other European countries, such as Switzerland, have also adopted this regulation.
Operating systems and machines in areas with potentially explosive air, gas, or air/dust mixtures require special procedures.
If such a mixture formation cannot be prevented, specially protected gear units must be used. Applicable standards and regulations
govern the use of equipment within existing hazard zones. They also prescribe the quality prerequisites that must be met
by drive manufacturers.
The explosion-proof industrial gear units of the MC and X series and the planetary gear units from SEW-EURODRIVE meet the
design requirements for group II, category 2G or 3G (potentially explosive gas atmospheres) and 2D or 3D (potentially explosive
dust atmospheres). The gear units are suitable for use in zones 1 and 21 or zones 2 and 22.
|
| back to top |