www.sew-eurodrive.com

Login
 
You are here: Home >
Winding calculator
Products
Drive application: Winding calculator
Winding calculators are used when endless material is unwound for further processing or rewound after processing. This may be necessary e.g. in the paper, plastics, textile or sheet metal industries. It is very important that the speed of the material transport remains constant. The speed of the material roll is changed in inverse proportion to its radius. To prevent the material from tearing, it is wound smoothly and the tension must be kept constant. The following description of the drive solution is based on two unwinders.


The solution with MOVIDRIVE®
Connection via system bus
The MOVIDRIVE® solution assumes that each unwinder and pull-off roller is driven by its own motor. Both MOVIDRIVE® drive inverters are connected with the standard system bus (SBus). External encoders on the line can be avoided through the data exchange between the inverters. The inverter can recognize possible band tearing. An automatic threader ensures that the process continues as soon as possible.


Guide with jockey roll
In the case of clocked further processing, the guide around the jockey roll is extended. The jockey roll acts as a buffer to compensate for the tensile force fluctuations and load shocks arising from clocked operation. The position of the jockey roll is entered with a potentiometer and the signal is forwarded to the MOVIDRIVE® of the winder.



IPOSplus®
A significant feature of the MOVIDRIVE® drive inverter, the IPOSplus® positioning and sequence control system, now comes into play. It turns the MOVIDRIVE® into a real winding calculator. An IPOSplus® program in MOVIDRIVE® calculates the setpoint of the torque or the setpoint of the unwinder speed based on the speed of the unwinder and pull-off rollers and the specified valid tensile force (for example, via the fieldbus of a PLC).



The benefits at a glance


 
back to top