www.sew-eurodrive.com

Login
You are here: Home > Documentation \ Software \ CAD > Software Result
Software
...or choose the software directly here:
Order:
The following articles will be sent to you as quickly as possible (max. 15 pieces if documentation was ordered).
   
Download
   
 
Result:
 
GSDML for PROFINET IO MOVIDRIVE® MDx61B + DFE12B  
version: 1.0 - 20050318
Unit master files are required to connect PROFINET IO stations to a PROFINET fieldbus system.

Further information is available in the manual "MOVIDRIVE® MDX61B Fieldbus Interface DFE12B PROFINET IO".

0,01 MB
back to top