www.sew-eurodrive.com

Login
You are here: Home > Documentation \ Software \ CAD > Software Result
Software
...or choose the software directly here:
Order:
The following articles will be sent to you as quickly as possible (max. 15 pieces if documentation was ordered).
   
Download
   
 
Result:
 
LT Shell for PDA (Windows CE)  
version: Version 3.51 - 23.07.2009
With LT shell for PDA parameters of Movitrac LT can be changed and stored via PDA or pocket PC. Version 3.5 or higher requires NET Compact Framework 3.5 or higher. www.microsoft.com

0,37 MB
back to top