Order:
The following articles will be sent to you as quickly as possible (max. 15 pieces if documentation was ordered).
Download
Result:
CAD data for DOP operator terminals
Includes CAD data in IGES and DWG format for the following DOP operator terminals: DOP11B-10, DOP11B-15, DOP11B-20, DOP11B-25+30, DOP11B-40, DOP11B-50, DOP11B-60