Order:
The following articles will be sent to you as quickly as possible (max. 15 pieces if documentation was ordered).
Download
Result:
MOVITOOLS® MotionStudio 5.60 SP2 Compact
version: 5.60 - build 5.6.0.10 Compact version
- without MOVITOOLS®
- without PLC Editor
This data-reduced version offers all subroutines required for startup and diagnostics of the following units:
- MOVITRAC® B without using IPOS sequence control
- MOVIAXIS®
- MOVIGEAR®
- MOVIFIT® function level Classic
- Fieldbus gateways type DFx